How can i get the schemetic of MB1440B by STLINT V3 set ?
Hi: Mostly the Stlink V3 set seems like a develop board , i am realy need more information about the MB1440B , So how can i get the schemetic ? thanks a lot .
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hi: Mostly the Stlink V3 set seems like a develop board , i am realy need more information about the MB1440B , So how can i get the schemetic ? thanks a lot .
Dear Sir, We are manufacturer of hotel automation products in India. We intend to use ACST (AC Switch Triac) in two applications. For On/Off control (to replace electromechanical relays) and for phase control of light / fan dimming application.We wis...
INTERRUPT_HANDLER(USART1_TX_TIM5_UPD_OVF_TRG_BRK_IRQHandler,27) { /* In order to detect unexpected events during development, it is recommended to set a breakpoint on the following instruction. */ USART_SendData8(USART1, TxBuffer[T...
HelloI need to design an EFT filtering circuitry in front of the DC-DC power lines to suppress industrial transients, according to standart IEC 61000-4-4.I need performance criteria A (device is not affected any of the transients) suppression for at ...
Sorry if its wrong section to post this.I found this IC from a Galaxy Note 4, apparently it has something to do with display. My display isnt working because this IC is blown. This is what it looks like:Code on top reads : ST 328 M515It is very small...
Where can I get datasheets and manual on this MCU : ST10F296M-A1 ?Further numbers on it: VG023240 992DH MYS 22 035Closest I found was a doc CD00211833, ST10F296E (which seems like, a device user manual?)And nothing else with the exact number is prin...
when i am using 8 bit microcontrollers, i use compilers that have a lot of libraries to make my work in programming the micrcontroller very easy, e.g lcd library and a lot of libraries so the development of my code will be easy, in fact i am trying t...