Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIMER 1 channels in OC mode.

Hello! I'm learning to code an STMicroelectronics 8 bit micro-controller. I want to control a BLDC motor with this MCU for electric vehicle application. I'm using the STM8S DISCOVERY Board, based on the STM8S105C6T6 (48 pin) MCU. This MCU has 4 timer...

0690X00000AQLE6QAP.jpg 0690X00000AQLE1QAP.jpg
DebD21 by Associate
  • 2058 Views
  • 0 replies
  • 0 kudos

Weird bug in stm8 IAR compilers ?

Hi.I have faced a weird problem using IAR compilers.Errorstatus=0; Relay_Off; delay_ms(200); if(Errorstatus==1){ Errorflag=1;In this part of my code after I switch the relay off, I put a delay and if an interrupt...

Program the STM8 MCU(SWIM) using Nucleo-L152RE

I have Nucleo-L152RE board and I used this board to program the STM32 MCU using JTAG (CN4) connector. Now, I want to program the STM8 board using SWIM interface. So, is it possible with Nucleo-L152RE?. I already done the required changes to use Nucle...

AP_040 by Senior
  • 4216 Views
  • 6 replies
  • 0 kudos

[ST10F269]Interrupt Handler is not working

When I develop the digital communication board using the ST10F269, I see the problem.- Problem: Although the interrupt signal is normal, interrupt handler of ST10F269Z2T3 is not working.I want to receive the advice about this problem.Q1) What is the ...

CKim.0 by Associate
  • 679 Views
  • 0 replies
  • 0 kudos

Hi, Can ECMF02-2AMX6 used for USB 3.0 application.

Can you also confirm how many pins have inbuilt ESD diode? According to datasheet its 2. But according to diagram in datasheet 4 pins have ESD.Also suggest which choke is better for USB 2.0 and USB 3.0 application among these two.ECMF02-2HSMX6 or ECM...

SN.10 by Associate II
  • 777 Views
  • 1 replies
  • 0 kudos

timer counter

float get_resi(void) in https://gist.github.com/goog/bf784c5f63a199ddbde7cd49db92f73fcould you help to check the get_resi function?im not sure whether my time counter has some issue?

Thank you for allowing me to join. I am looking for technical data for a Thyristor, Particularly the operating temperature of the device.

The details on the device are ST DS(5)NM6 0(O) 6K0(O)8H222 I have indicated in brackets the option for the read symbols on the device as I may have misread them. This device is fitted in a Carlo Gavazzi DMB01C timing relay and it appears to ...

MWalt.8 by Associate
  • 991 Views
  • 1 replies
  • 0 kudos