Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hello ST,I can't find any information for the correct package marking (part marking) of eeprom M95128-DRDW8TP/K.Data Sheet for this device not includes information about package marking specification.On the ST site for this device also has no informa...
I'm trying to use the emulated EEPROM on the b-l475e-iot board... I'm following the example from X-Cube-EEPROM, and everything looks ok... when it goes through storing values and then reading them back, everything matches... but if I try to read the ...
Hello everybody,I am experiencing an unexpected power consuption from the STM6600CS25DM6F. When the button is pressed an extra amount of current is drawn (40uA) from the circuit. I know that some of it is due to the pull-up resistor on the pbout pin ...
Hi. I'm glad you're reading this, i hope you can help.Click-bait aside, i experience a nasty and unexpected behavior of external interrupts in a professional, industrial product designed around STM8AL318ATC.In short, there are 2 digital signals (from...
#include <stdint.h>#include<iostm8s.h>void main(void){ TIM2_PSCR = 0b00000111; TIM2_EGR= 0x01; TIM1_CR1 = 0x01; PD_DDR = 0x01; PD_CR1 = 0x01; while(1) { if ( ( ((uint16_t)TIM2_CNTRH << 8) + (uint16_t)TIM2_CNTRL ) >= 15625 ) { TIM2_...
INTERRUPT_HANDLER(USART1_RX_TIM5_CC_IRQHandler,28) { /* In order to detect unexpected events during development, it is recommended to set a breakpoint on the following instruction. */ //uint8_t temp = USART1->SR; ...
I'm trying to connect an external antenna to the B-L475E-IOT01A1 eval board...The data sheet says that the external antenna is designed to be used with the U.FL connector...but I can't find is whether the U.FL connector is already soldered onto the b...