Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S003F3U outputs behaving weirdly during BOR.

I have been working on a battery powered application and am experiencing some strange behavior when the batteries are dying. The LED array is being driven by a PWM signal on PD4 through a FET. When the +4V power line goes down to 2.6xx V, all of th...

KDesr.1 by Associate III
  • 3262 Views
  • 5 replies
  • 0 kudos

UART Even Parity gives parity error

Hi,I'm using STM8S for UART half duplex communication (single wire). I'm using the standard library to set the UART up in 9600 baud rate, 8 data bit, even parity and 1 stop bit. I recieve data using interrupts. On the third byte, I get a parity error...

DDeba.1 by Associate III
  • 2213 Views
  • 2 replies
  • 0 kudos

How to generate firmware for STNRGPF02

Hi everyone, I'm designing an application with an STNRGPF02 and would like to generate an appropriate firmware for it.I made the conception using the STNRGPF12 design, since the chips are very similar and the PF02 is not available through eDesignSuit...