cancel
Showing results for 
Search instead for 
Did you mean: 

How to generate firmware for STNRGPF02

Julien FAUCHER
Associate III

Hi everyone, I'm designing an application with an STNRGPF02 and would like to generate an appropriate firmware for it.

I made the conception using the STNRGPF12 design, since the chips are very similar and the PF02 is not available through eDesignSuite (even though the documentation says otherwise), but there is (obviously) no option for the relay inrush parameters and I can't be sure that it will work properly (which I would rather know before testing a non isolated, line powered application :grinning_face_with_sweat: )

Could someone tell me the appropriate way to proceed ?

Best regards,

Julien FAUCHER

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0