Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST VD Software installation Issue : An anomaly (1) has been detected during installation.

Hi Team,I have installed ST Visual Develop in ST web page. At the end of installation, installation page got stuck and then i have terminated by end task using task bar....After completion of installation, i have opened software then following error ...

STNRG328 Bootloading procedure

Hi All,​There are a questions about AN4656 Application note,while I am trying Access EEPROM by following this document.Where is the file(*.s19) mention in Chapter 8 .I have been searching on the ST official website, but found nothing.How do I obtain ...

CHsia.2 by Associate
  • 914 Views
  • 0 replies
  • 0 kudos

Resolved! Applying voltage to the output pin of STMPS2171STR

Hi,Currently, I have two boards that contain a 5 volt power supply. Due to flexibility for future projects, both of are powering the same pin on a connector. The STMPS2171STR was added to one of the boards to cut the voltage going to the connector. H...

MOliv.1 by Associate II
  • 1813 Views
  • 7 replies
  • 0 kudos

Truth Table for STHV800L?

Hi,the included data brief in ST site does not provide the function of input pins. Like a truth table as to how to control different channels I was wondering if someone can provide me with the same..Thanks in Advance.Thanks and Regards,Siva

SSR by Associate
  • 725 Views
  • 1 replies
  • 0 kudos

STM8 Eclipse device descriptions (XLM/SVD)?

hello all,I am currently trying to add STM8 peripherals to the Eclipse embsysregview plugin. For this I would need device descriptions in XML or SVD. For STM32 ARM devices these are published as SVD files (see e.g. https://www.st.com/content/st_com/e...

GIcki by Associate II
  • 5075 Views
  • 4 replies
  • 1 kudos

Resolved! EEPROM WriteProtection

hey allI am using EEPROM library in the link belowhttps://github.com/sinadarvi/SD_HAL_AT24/blob/master/at24_hal_i2c.cI used the code successfully and it worked properly. I am using AT24C32. there is a WriteProtection pin on it, without enabling it, ...

Ala by Senior
  • 1252 Views
  • 1 replies
  • 0 kudos