Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN example for STM8A Discovery?

I am looking for an CAN bus example for the STM8A discovery board. App Note 4178 (LIN example) refers another App Note (4179) for a respective CAN example. However, I can't find it on st.com - nor can I find a suitable example via Google. Can someone...

GIcki by Associate II
  • 1066 Views
  • 1 replies
  • 0 kudos

DNP3 implemetation

Hi everyoneI need a library for ARM to implement DNP3 protocol. does anyone here know how should I do it? does send/receiving DNP3 packets make it possible?

Ala by Senior
  • 1120 Views
  • 0 replies
  • 0 kudos

Dear people of ST Microelectronics For a school project I would like to use the IGBT STGW40M120DF3 from ST Microelectronics. Is it possible that the TestCircuit in the Datasheet is the real setup and not a possible PSPICE TestCircuit? Kind regards

The data sheet contains the following TestCircuit:I wanted to use it to check the switch in PSPICE. Unfortunately I don't get the same results as in the datasheet. If my assumption is correct: Could you give me a TestCircuit for a PSPICE circuit wher...

UFisc.1 by Associate
  • 632 Views
  • 0 replies
  • 0 kudos

I'm trying to read an ADC(channel 7) which is the internal reference voltage channel for stm8s903f3, to print the adc value read on uart terminal. But for some reason its not continuously printing the adc value that is being updated.

It updates if I manually reset the board. I'm setting my baudrate as 11400, but it works only if I select the baudrate as 115200 on hyperterminal. Here is a snippet of what Im working on. (EDIT) It even works when I step through the code, not when I ...

PMoop.1 by Associate II
  • 822 Views
  • 0 replies
  • 0 kudos

PROBLEM BY PC7 GPIO in stm8S003F3P6

HIi have connected a stm8s003f3p6 to a common anode 7segment.one of segments has connected to PC7 gpio and it is always on because PC7 does not drive to high level voltage.it would be appreciated if help me?thanks

Amous.1 by Associate
  • 1603 Views
  • 3 replies
  • 0 kudos