Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The problem is that the controller of stm8 doesn't work after it has been used on the vehicle for a period of time, and the controller function is invalid. Once in the past, the controller can work normally after re burning the program, but this time ther

The problem is that the controller of stm8S208C8T6 doesn't work after it has been used on the vehicle for a period of time, and the controller function is invalid. Once in the past, the controller can work normally after re burning the program, but...

Wzhan.5 by Associate
  • 1194 Views
  • 1 replies
  • 0 kudos

STM8AL3189 flashing of image on address above 0xFFFF that code is not working and using STVD tried

Hi Team,I am using the STM8AL3189 controller, created 2 images where,1st image will flash with 0x8100 to 0xffff and 2nd flashing of the image will flash on 0x10000 to 0x17fff (address above 0xFFFF )we have changed the linker file with the startup fil...

0693W00000AMQ3oQAH.png

STM8L050J3 SON8N - how to generate PWM on PC5 ?

Hello,I am trying to generate a PWM signal on pin PC5 using TIM2_CH1 , but no success. But I am able to generate PWM on pin PD0 using TIM3_CH2.Normally the procedure is quite simple :for TIM2_CH1 - pin PC5 TIM2_OC1Init(TIM2_OCMode_PWM1,  TIM2_OutputS...

0690X000009Yx7yQAC.png 0690X000009Yx7jQAC.png
SDomn by Associate
  • 1345 Views
  • 3 replies
  • 1 kudos