Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hello, I'm writing some timer code for the STM8S003F3P6. I am using SDCC to compile it and stm8flash to flash it on to the device with a third part ST-Link V2. I am having an issue that when I flash the device with my code it doesn't run and I can no...
I did not understand that VCC range of the SRC0CS25D is 1V6-5V5 and the electrical specifications state Vth=(min,type,max)=(3v29,3v40,3v50). There is some uncertinity about the thereshold. If my VIN voltage (given to VCC pin of SRC0CS25D) is under 3....
In the STM8L SDK, the RTC_WakeUpCmd() function can return an ERROR if the WUTWF bit fails to be set after a delay. In the RM there's no mention of how and why this situation would occur.Why RTC_WakeUpCmd can fail?Thanks,Gabriel
I would like to protect my firmware and my microcontroller in the case of a user want to extract the hex file or if the user want to overwire my firmware. For the first case, I saw I must play with 2 registers before to compile and program my code. H...
Hi.i'm try using USART1 and recieve bytes with DMA from SBUS transmitter.. But have strange problem - i'm recive only once and later DMA IRQ TC2 never occure. I'm try many variants - all not help me(((Here my some code - #define USART_DMA_CHANNEL_RX ...
I'm specifically interested in PSD813F2A-90MI. Is it possible to get the last released statements?
It is for a veglia boreti automotive instrument cluster from a fiat punto 2001 - 1999Hi there! I wanted to politely ask for your help, if you can answer a simple question: i have a 950406 k128 eeprom chip but cant find one to buy online i only can fi...