Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L DMA and ADC out of sync?

I have STM8LDiscovery (with STM8L152C6T6 CPU). I need to continuously read 2 ADC channels with writing the data to the memory.I'm doing my project in IAR EW for STM8 v. 3.11.4.I run into the problem: channels data (ADC_DATA) continuously exchanging t...

rmatveev by Associate II
  • 2426 Views
  • 3 replies
  • 0 kudos

Query regarding metering accuracy

Good day, Support TeamI'm working on a single-phase Panel meter. Which provides import and export of both energy sources on ModbusFor metering purposes, we are considering the STPM3x family of ICs (STPM32, STPM33, STPM34).I've attached one image from...

0693W00000bhGUuQAM.png

Resolved! STM8 UART2, Adding a parity bit to UART packet

I am attempting to configure the UART2 peripheral of the STM8S105C4 MCU with an even parity control using this development environment: ST Visual Develop, ST Visual Programmer, STM8 Cosmic compiler, Library: STM8 Standard Peripheral Library (SPL).Pro...

0693W00000bhF8OQAU.png
Kmax18 by Senior II
  • 2557 Views
  • 2 replies
  • 2 kudos

Kindly fill the attached fo22 form.

Dear Team,Hope you are doing good.This mail is regarding to fill the declaration form for REACH,ROHS, BATTERY SUBSTANCE RESTRICTION, INDUSTRY RESTRICTED SUBSTANCE, OTHER LEGISLATION, PROP 65, CLP, BPR. Kindly declared the mentioned regulation in the ...

AMahe.2 by Associate
  • 1614 Views
  • 1 replies
  • 0 kudos

Resolved! M24256-DRMF3TG/K Footprint

What is the recommended footprint for this device?The TN1171 technical note is next to useless, so please don't direct me there.What is the width of this pad please, as I cannot decipher your data sheet for this information  Frankly, I'm a little dis...

0693W00000aJqpwQAC.jpg
TScot.3 by Associate
  • 1210 Views
  • 3 replies
  • 0 kudos

Resolved! STM8S105C4T6, inverting the UART2_TX signal

I need an active high UART signal. Yes, the STM8S UART2_TX signal is active, but for hardware reasons I must invert the active low PCB output (UART2_TX). An easy solution would be a programmable STM8S feature to invert the signal. The reference manua...

Kmax18 by Senior II
  • 2131 Views
  • 3 replies
  • 1 kudos