cancel
Showing results for 
Search instead for 
Did you mean: 

VNI8200XP - SPI command activates valves only for <500ms.

LTubb.1
Associate

+24V Supply, 16-bit SPI, I send the proper bytes to activate valve 1-8, the proper LED(s) is activated as expected, but only for a short period, then it turns off. The driver responds with the correct byte, no errors, parity check is clean. WD_EN is pulled to Ground, Enable pin is high. Any ideas?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0