cancel
Showing results for 
Search instead for 
Did you mean: 

I think there is a bug in the STM32CubeIDE Version: 1.4.0 Build: 7511_20200720_0928 (UTC), section “device configuration tool�?, section STMicroelectronics.X-CUBE-TOUCHGFX.4.15.0 Mode and configuration.

AGendrau
Associate

When Graphics Application is checked, a folders tree starting from TouchGFX, with files like GFX2.touchgfx, etc, is generated. It’s OK.

When the .ioc file becomes complicated (as the example I attach), it seems that TouchGFX is replaced by Src and all files are generated under Src, mixing them with main.c and the other files.

Could you fix this, please?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Patrizia BELLITTO
ST Employee

Hello,

sorry but this is not the correct category for this question...please, try to move it under STM32 Q&A pages.

Regards,

Patrizia