cancel
Showing results for 
Search instead for 
Did you mean: 

AS21P2TLR peak switching energy

MSchi.3
Associate

I have a capacity of 40nF on the S2 pin, charged to a voltage of 3.3V.

The D pin is at GND. The 40nF is then discharged through the analog switch. The peak current will be around 6.6A for a very short time (if the analog switch has 0.5 Ohm resistance). But the datasheet specifies 500mA max. Will the analog switch survive that?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The 500mA in the datasheet refer to a pulse of 1ms with 10% duty cycle, which corresponds to an energy of 1ms * 0.5²A² * 0.5ohms = 125µJ, which heats the component, but which can cool down in the following 9ms of the duty cycle.

The 40nF capacitor only stores an energy of 218nJ at 3.3V and loses about 216nJ in the first 48ns with the typical switch-on resistance of 0.5 Ohm until it reaches a current of 0.5A and a voltage of 0.3V.

I don't see any issue if you repeat that with a max frequency of e.g. 200Hz.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

The 500mA in the datasheet refer to a pulse of 1ms with 10% duty cycle, which corresponds to an energy of 1ms * 0.5²A² * 0.5ohms = 125µJ, which heats the component, but which can cool down in the following 9ms of the duty cycle.

The 40nF capacitor only stores an energy of 218nJ at 3.3V and loses about 216nJ in the first 48ns with the typical switch-on resistance of 0.5 Ohm until it reaches a current of 0.5A and a voltage of 0.3V.

I don't see any issue if you repeat that with a max frequency of e.g. 200Hz.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.