Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB002 demo code download

Hi all,we have a P-NUCLEO-USB002 kit, and there is a pre-programmed demo image on kitthe demo image will output CLI to operate, (please refer to the attached picture.)but there is not found in the STUSB010 library.could you share the information of w...

qqGHUAN by Associate II
  • 2118 Views
  • 1 replies
  • 0 kudos

Cant download X-CUBE-SUBG1

I can't download the X-CUBE-SUBG1 library from the link:https://www.st.com/en/embedded-software/x-cube-subg1.html Other things download without problems.

mJar by Associate
  • 1088 Views
  • 0 replies
  • 0 kudos

binary and invert converion

i am sending data on serial is 3 when is display is this 3 but i can conver in bninary then become 00110011 instead 00000011.and when i invert it then i got 01100110 instead of 11111100 ,why so ?

MCU - suggestions

Hello STM!GOOD Day,We are looking new MCU for VOIP[voice over Internet protocol] project that can handle Internet connectivity and Communications like[ADC,UART] [,LAN, WAN, FXS, FXO support]. and  we are looking HIGH speed  MCU.  Thanks,Hari. 

hT.1 by Associate
  • 1390 Views
  • 2 replies
  • 0 kudos

STM32 Compile Error!

StmCubeIDE içinde yazılım esnasında kullandıgım cubeMX den bacak degişimi yaptıgım zaman, derleme sonrası sadece ana sayfa üzerindeki (main(void) içindeki...) kodlarım neden siliniyor? 

tayfun34 by Associate
  • 1380 Views
  • 1 replies
  • 0 kudos

Resolved! USB issue with STM32F411

This has nothing to do with EEPROM devices, but that was the only "labeI" that would work. I built a custom board using an STM32F411RET6. It has a 12MHz external clock. I'm trying to use a VCP USB interface. The USB code enumerates fine on a 'F407 DI...

marcmign by Associate
  • 2493 Views
  • 2 replies
  • 0 kudos