Dali 2 library.
Hello everyone,Does ST has Dali 2 library available for his customers?Best RegardsKarol
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hello everyone,Does ST has Dali 2 library available for his customers?Best RegardsKarol
Hello, can u suggest any part number which has specification with Allegro: A89307KETSR-J IC.As i want to design Software less BLDC FOC single shunt motor control solution.See the requirement as bellow,Operating temperature range: -40C to +100C Opera...
Hi,I've downloaded the following libraries for the modbus tcp/ip communication:https://www.st.com/en/embedded-software/stsw-stm32070.html the experimental setup is a slave: a board with stm32f407 and a switch:https://www.microchip.com/en-us/product/k...
I am applying the circuit in the picture I uploaded and when I touch the pin with my hand or touch it with a metal piece, the external break pin is triggered spontaneously. Please help me.
Respected Sir/Mam, 1) I am unable to find the spice models of the SiC Mosfet-SCTWA35N65G2V, Can anyone provide the spice model for this IGBT.and 2)THE SPICE model given for IGBT-STGWA50HP65FB2 after importing, while running in LTSPICE it is showing...
buon giorno a tutti sapreste indicarmi che tipologia di diodo è questo l'unica cosa e che è bidirezionale per il resto non riesco a trovare nessun datascheet
Hi,Thanks for using ST products. The X-NUCLEO-NFC02A1 expansion board is in Non Recommended for New Design status (NRND). I would recommend to move to active products such as X-NUCLEO-NFC07A1.Anyway, an X-CUBE-NFC2 firmware package is available for t...
I am using STM8S003F3. If the supply voltage of STM8S003F3 is 3.3v, the ADC works well.However, if you apply a supply voltage lower than 3.3V, the ADC will not work.I hope the ADC works well at 3.0V.For reference, I know that the minimum supply volta...
What are the functions of the two interrupt pins on the LSM6DSOX IMU sensor, and how does increasing the voltage of the INT2 pin affect the accelerometer’s Z-axis value?
Can i know the minimum Operating temperature of this IC "STTH112A-TR"will it support negative temperature "-40"