firmware choice for STEVAL-STWBXCS1
hi all,which firmware to use for STEVAL-STWBXCS1? datalog2 or ai monitor?regards,
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
hi all,which firmware to use for STEVAL-STWBXCS1? datalog2 or ai monitor?regards,
HiI am using the MAX17261 fuel gauge IC and my MCU is STM32U5G7VJTXQ. According to fuel gauge's datasheet, the ALERT pin (active low pin) is asserted under the following conditions:SOC changeSOC crossing minimum or maximum thresholdsVoltage crossing ...
Hi everyone,I’m currently working on a design to integrate an ESP32-C6 with the ST85MM PLC modem, and I’m hitting a few roadblocks regarding the best hardware architecture and communication flow.To be honest, I'm also a bit confused about the specifi...
Hello everyone,I’m working with an STM32F103C8T6 (Blue Pill) development board and facing an issue while trying to program/debug the MCU using ST-Link V2.Board used:https://robocraze.com/products/stm32f103c8t6-arm-development-boardIssue details:STM32...
Title edited to flag that this relates to a Blue PillI'm trying to connect an STM32-STLink-V2 with three wires via SWD (GND, SCLK,SDIO). Was able to run a firmware upgrade, now V2J46S7.Clicking on Connect gives:15:35:11 : UR connection mode is define...
Hello,I use a STSAFE-A110 chip on a own board based on STM32 MCU.As I was unable to integrate the STSAFE library provided by ST on my specific fw, I wrote features whom I need as as echo, generate random, retrieve product data, generate host key, ret...
I have been using Scool together with Keil for years, but last tuesday after I started my PC and a win11 update was installed, I started Scool but got this error: "The PC/SC access cannot be enabled for the reader (driver not installed?) SdtReaderDll...
Title edited to correct part number: it is a Geehy APM32F103CBT6 - not an STM32.See this post.Hi everyone,I am working on a project using the STM32F103CB MCU and implementing Standby (low-power) mode in the firmware. Development is done using Arduino...
Hello,I am trying to integrate an STSAFE-A110 chip into my product for keys/data securely storage.The communication with the chip works fine (approved by simple command as echo or generate_random).So I tried to generate a key in a local envelope key ...
We have provided SWIM, 5V, and GND connections to the microcontroller for programming and debugging purposes. Is it possible to program the ST8S001J3M3 MCU using the ST-Link V2 or V3 via the 5V, SWIM, and GND connections?Please find the attached refe...