Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PA4 and PA5 don't work STM8S208RB

Hello,STM8S208RB microcontroller. Pins PA4 and PA5 do not work in push-pull mode. Why? I haven't tried it in other modes. It's not a microcontroller issue because I tested it on two different microcontrollers. Pins are shown in the datasheet (see fig...

MykolaLevun_0-1711293982148.png

Resolved! Diode BEK19A

Good evening, I am not founding data scheet of this diode BEK19A, maybe obsolete. Can some one provide analog datas cheet diode please?

SMusc.1 by Senior
  • 8919 Views
  • 8 replies
  • 3 kudos

Resolved! Top Side part marking for M24C08-FMH6TG

Hi I am looking for the top side park marking of component M24C08-FMH6TG.Is this something I should be able to locate myself? I checked the datasheet and engineering notes for the package type.Thank you so much.-Ben

BFST7676 by Associate II
  • 2353 Views
  • 4 replies
  • 3 kudos

STVisual Develop simulator without STLink?

ST visual Develop Version 4.3.12!  running on Windows 10.I have set this up with the Cosmic toolkit and can build images for my ST8 processor but can I run the simulator without STLink?Apologies for such a newbie question - first time I've tried to d...

STEVAL-FKI915V1(S2-LP)

Hello!I would like to test it using STEVAL-FKI915V1(S2-LP).-. Setting conditions:1) Frequency used: 924.6MHz2) Channel Bandwidth: 10KHz3) Modulation Mode: CW4) Temperature: 255) Applicable register: see attached file.Questions1. EV BD (STEVAL-FKI915V...

JDSOFU2 by Associate
  • 1235 Views
  • 0 replies
  • 0 kudos

How to read and write M24256-DFCS6TP/K EEPROM

Hi, We are using STM M24256-DFCS6TP/K 256-Kbit serial I²C bus EEPROM. We want to read and write the whole memory inside the EEPROM data. Are there any commands available in the u-boot and kernel test? and also if I want to read a particular location ...

I'm Facing Some Serious issue on RC522 To STM32

// Waiting to receive data to complete i = 2000; // i according to the clock frequency adjustment, the operator M1 card maximum waiting time 25ms do { // CommIrqReg[7..0] // Set1 TxIRq RxIRq IdleIRq HiAlerIRq LoAlertIRq ErrIRq TimerIRq n = Read_MFR...

Major_Man_0-1710939198466.png Major_Man_1-1710939242509.png