Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Top Side part marking for M24C08-FMH6TG

Hi I am looking for the top side park marking of component M24C08-FMH6TG.Is this something I should be able to locate myself? I checked the datasheet and engineering notes for the package type.Thank you so much.-Ben

BFST7676 by Associate II
  • 2413 Views
  • 4 replies
  • 3 kudos

STVisual Develop simulator without STLink?

ST visual Develop Version 4.3.12!  running on Windows 10.I have set this up with the Cosmic toolkit and can build images for my ST8 processor but can I run the simulator without STLink?Apologies for such a newbie question - first time I've tried to d...

STEVAL-FKI915V1(S2-LP)

Hello!I would like to test it using STEVAL-FKI915V1(S2-LP).-. Setting conditions:1) Frequency used: 924.6MHz2) Channel Bandwidth: 10KHz3) Modulation Mode: CW4) Temperature: 255) Applicable register: see attached file.Questions1. EV BD (STEVAL-FKI915V...

JDSOFU2 by Associate
  • 1261 Views
  • 0 replies
  • 0 kudos

How to read and write M24256-DFCS6TP/K EEPROM

Hi, We are using STM M24256-DFCS6TP/K 256-Kbit serial I²C bus EEPROM. We want to read and write the whole memory inside the EEPROM data. Are there any commands available in the u-boot and kernel test? and also if I want to read a particular location ...

I'm Facing Some Serious issue on RC522 To STM32

// Waiting to receive data to complete i = 2000; // i according to the clock frequency adjustment, the operator M1 card maximum waiting time 25ms do { // CommIrqReg[7..0] // Set1 TxIRq RxIRq IdleIRq HiAlerIRq LoAlertIRq ErrIRq TimerIRq n = Read_MFR...

Major_Man_0-1710939198466.png Major_Man_1-1710939242509.png

STEVAL-SPIN3202 not driving custom BLDC motors

I am using STEVAL-SPIN3202 to drive BLDC motors other than specified in the user manual - Bull-Running BR2804-1700 kV, RS Pro 57BL54 and Faulhaber Minimotor 2036U024B. No error messages observed in ST Motor pilot. But motor does not spin.Let me know ...

sskr by Associate
  • 781 Views
  • 0 replies
  • 0 kudos

Resolved! I/O circuit

Hey there , how can I find info to conect my STM32 with higher voltage devices , for digital inputs and outputs I have 24vcc and analogic inputs and outputs -10 to 10v, I want to conect they safely to not burn my chip.

Chris8 by Associate II
  • 4959 Views
  • 5 replies
  • 0 kudos

Resolved! UAA4003DP Chip Alternative

I am looking for a alternative chip to replace an obsolete part.The part is a ST UAA4003DP This a 16 pin chip used in a DC motor drive to control the motor speed.I can't find any information on this other than the fact that it is obsolete.. I did fin...

tsteg by Associate
  • 1624 Views
  • 2 replies
  • 1 kudos