Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need clarification on PCN

Will you please confirm on below part numbers that whether there will be any change in electrical parameters of the affected MPN depending on their PCN. For that do we need to verify any electrical parameters again?  Part TypePCN Tracking NoType of C...

Technical issues related to RF transistor SD2933

We want to use this transistor to drive piezoelectric ceramics at 900KHz, 1.7MHz, and 3MHz, which requires about 50W of power.I have the following questions and need help:1. Can this transistor be used at a frequency of 900kHz? Can it only be used in...

H_YM by Associate II
  • 2003 Views
  • 1 replies
  • 0 kudos

Reading STUSB4500 USB PD status via I2C

The USB PD status register is a combination of 4 registers.The question is when read, are they interpreted as big endian or little endian?so 0x91 0x92 0x93 0x940x91 = bit 0-7, or 28 - 31?0x92 bit 8-110x93 ...0x94 ...The manual and programming guide a...

fbrown by Associate
  • 1706 Views
  • 1 replies
  • 0 kudos

STUSB4500 damaged during reconnection

Hi,We have a custom implementation based around STM32H7 and STM32F1.The application is powered internally by a rechargable 4s li-ion battery.We use USB-PD to charge the device, and USB 2.0 to communicate with the STM32H7 through an external ULPI-PHY....

STUSB4500-implementation.png
LFjær.1 by Associate
  • 2961 Views
  • 3 replies
  • 0 kudos

Resolved! 632565 9303

Trying to find details about this chip. New to this and trying to follow tips to fix a car. This chip i was told was going to be a 93xxx series eeprom but as you can see its not. I cant find anything on it looking up the part number unless im missing...

karl2 by Associate
  • 3098 Views
  • 3 replies
  • 0 kudos

AN2659, chaining interrupts, how?

AN2659, section 4.1.3 Vector table redirection, says that "The primary interrupt table contains a set of jumps to the user interrupt table" but the same code that accompanies this document does not seem to implement this - does this code just need to...

Resolved! 74LCX541/SO

Hello Everyone,I am facing problem in ADC section of  our project schematic. We are using ADS8505 Analog to digital converter as the output of ADC ranges from 0v to 5V and microcontroller which we are using(STM32F413ZGT6) is connected to 3.3 Volts su...

Rushali by Associate III
  • 3861 Views
  • 4 replies
  • 1 kudos