Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST MFU C104 diode info.

Help please!I'm unable to find any info on this diode from an old Siemens Siplus 24RCL PLC controller.  Pictures attached.The diode shorted closed.  I'm assuming because, someone hooked up the supply backwards!The only marks I've found are "ST MFU C1...

Kendog by Associate
  • 1176 Views
  • 2 replies
  • 3 kudos

TS514IN

Is this part Non-Rohs? Date Code 0234.  I see the newer part TS514AID look to be Rohs. Where can we look up part's to see if they are Rohs or Non-Rohs?  

BXion.1 by Associate II
  • 304 Views
  • 1 replies
  • 0 kudos

Parameter Definitions of L9678P

Hi,I'm using L9678P. I’d like to confirm the specific definitions of these parameters:Is 1~10KΩ the detectable range?Are the conditions in the "Condition" column strongly correlated with the parameter values?What does "Equivalent to resistance range"...

Snipaste_2025-02-10_10-20-42.png Snipaste_2025-02-10_10-21-12.png
Yang1 by Associate
  • 360 Views
  • 1 replies
  • 0 kudos

Resolved! MIPI_DSI ESD protection

Hello, this is the ECMF4-40A100N10(MIPI DSI ESD protection). I want to implement it in my design and I was wondering if it matters to connect your positive differential pair signals to D1+ and D2+ and negative to D-. Or can  acually flip them? So I c...

DonPotokon_0-1738929627492.png

Resolved! Need TPM IC behavior model for develop

HI ST teams, I 've purchased STPM4RasPIV21 to test our SPI master device. I'v observed this TPM IC uses wait state when communication. Please help share behavior model(verilog) for SPI master simulation. Thanks a lot.

CYHou by Associate
  • 563 Views
  • 1 replies
  • 0 kudos