Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPM10 replacement since it's NRND

Hi all. I'm about to start a project where we just measure the voltage and current of a single phase 220V 50Hz line. We need all the usual values (P, Q, S, cos phi, etc) using a CT and a standard transformer for the voltage. We also don't care that m...

Cocus by Associate
  • 561 Views
  • 0 replies
  • 0 kudos

HCF4013 is can withstand 24V at 1Min test?

Hi sir,As per our application, we need to enable and disable the power supply IC enable pin. So we are using Flip flop based toggle function. so we are connect 12V rail directly (before voltage regulator).So as per ISO standard, our application shou...

VM.1 by Associate
  • 513 Views
  • 0 replies
  • 0 kudos