Hi ST,We are implementing an M24C02-DRMF3 EEPROM based design and wanted to confirm the correct package marking for this device including part number, die version, date code and fab facility. Although the Data Sheet includes the WFDFPN8 mechanical in...
Hi, I'm looking for what I think is a Mosfet with this print, see the attached picture.I need to replace it because it's burned, but I don't know the features.Anyone can help me about ?Thanks a lotIvano
I used to choose a 10K resistor.But something seems to been wrong. Can anybody help with this? please!
I am interested in using this part due to it's radiation tolerances. However, the datasheet posted online only explains the radiation and package specifics. There isn't anything describing the pin out and function of the part. Can someone forward ...
I am attempting to connect to an st10f276z5. I have power and ground to the device, PL0.4 tied low, and PL0.5 tied to 5V. ST10 Flasher produces a 'Bad acknowledgement value error. 0x?? instead of 0x5A' Where the read value 0x?? seems to come up diffe...
I am working on a LoRaWAN and GNSS project. I have found one inconsistent operation when try to configure UART1 for GNSS connection. UART2 is used as PRINTF for logging. Procedure to produce bug: Use I-CUBE-LRWAN example as the codebase.Add code fr...
Hi.Now I am composing the model of the device in the program Microcap using SPICE model of IGBT STGW20NC60VD. This transistor has current-voltage characteristics shown Figure 1. But SPICE model of transistor has other different characteristics (Fig. ...