Hi Franceso,I have created and SimOsGetPos application with STM32L073_Nucleo and X-NUCLEO-GNSS1A1.using cubemx with x-cube-gnss1a1 version 3.1.0 and after enabling debug option with Usart2 by #define GNSS_DEBUG 1 it is showing below message on termin...
picture attached
Looking for a replacement for M41T00CAP, which went obsolete in October.
Is there any driver for the VB6955CM camera module? I need to use it on Android, but there's no driver in the kernel.The VB6955CM camera module is used on some Nokia Lumia devices.
Hello,is looking for a symbol marking eeprom:Thank YouKrystian
The old M95256-W datasheet Rev. 6 says:"The M95256-W and the M95256-R devices (2.5V and 1.8V versions, processed in F8 andidentified with the letter "A") offer an ECC (Error Correction Code) logic"The new version Rev. 21 says:"M95256 and M95256-D dev...