Others: hardware and software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ACST310-8B in light dimming application

Hi,I wish to use ACST310-8B in light dimming application.1. As shown in typical diagram of Phase Angle control, in the datasheet of ACST310-8B, can we avoid using choke/inductor in series with load?I believe this choke/inductor is needed for di/dt pr...

0690X000009joQjQAI.png
DLoha by Associate
  • 362 Views
  • 0 replies
  • 0 kudos

Hi Team, i am using M24M02-DRMN6TP for one of my project. While working with this EEPROM, we have observed an odd behavior. Please consider this as urgent

When we wrote data at 0 location, same value getting reflected at 32768 and vice versa. Same behavior for 65536 and 98304, 131072 and 163840, 196608 and 229376. Not sure why it is writing at two locations same information even though we have written ...

ABCD by Associate II
  • 503 Views
  • 4 replies
  • 0 kudos

L9825 SPI Control Not Functioning

I am attempting to set the output states of an L9825 using its SPI interface, but no matter what byte is transmitted, the returned diagnostic byte is 0x88 and the output state is unaltered.clock frequency : 1 MHzclock polarity: lowclock phase: data c...

MBoren by Associate II
  • 385 Views
  • 0 replies
  • 0 kudos