Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Intelligent power module

*Is it possible to utilize just one phase from the SLLIMM high-power IPM, which is a 3-phase inverter with a 650V short-circuit rugged IGBT rated at 50A? Additionally, do you have an IPM comparable to the discontinued STGIPS40W60L1, a half-bridge IGB...

Resolved! Getting started with the STUSB4500QTR

I'm trying to get started with the STUSB4500QTR and at this point have not changed anything in the device but at the same time I am not using any of its capabilities. The attached schematic shows where I am now. The intent is that a PC (right now jus...

DavePfz by Associate III
  • 2946 Views
  • 4 replies
  • 0 kudos

STSAFE-A110 is bricked during initial programming.

Hello to the ST engineers or anyone familiar with problems when programming the STSAFE devices: We are seeing about 10% of our STSAFE-A110 devices permanently fail during initial programming. Per the guidance in Section 5.2 of the data sheet (linked ...

TimJ by Associate
  • 1023 Views
  • 2 replies
  • 1 kudos

FIT Data

Is there FIT data available for STPS30170DJF Schottky Diodes? Best regards, Martin Best

mpbbldr by Associate
  • 983 Views
  • 2 replies
  • 0 kudos

STG3692 Supply Voltage

Hi, I wonder if the analog switch STG3692 can be used with +5V. I have concerns because recommended voltage value is +4.3V in the datasheet while absolute maximum is +5.5V, is there any risks about thermal conditions at that level? What do you sugges...

black bill stm32f401cc swo feature enable .

i am working with black pill board  that uses stm32f401ccand i have a debugger that was attached to neucleo board stm32f401re and i broke it from the board , the black bill debug pins only have the ground and the 3.3 and the swsck and the swdio ,i co...

Resolved! Diode Zener

Hi, Im trying to track down a couple of diodes to repair a card.  The markings are  EV Z551 It also has the ST logo on it, surface mount..  Anyone know where I can obtain some.. Cheers Kev

Jamer by Associate II
  • 4545 Views
  • 6 replies
  • 0 kudos