2025-04-22 11:57 AM
Hi, I'm developing a Bootloader for SPC58, If I full secure the micro and put its LC status as In-Field on UTEST, is there a way from the internal code (I can implement a serial command for the purpose) to unlock the JTAG? Or there is no way animore?
Best regards
GMG
2025-04-26 1:00 PM
Can someone from ST give a feedback ?
2025-04-26 6:28 PM
Perhaps this is an issue you'd need to discuss with your direct point of contact, or you FAE (Support Engineer) responsible for your account.
Alternatively you might need to pose this via an Online Support request on the OLS system?