Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SRAM faut injection

Posted on December 11, 2015 at 11:31Hello everybody,I'm working on the SPC56EL70L5 From the reference manual, I know that:“For platform RAM, the intent is to generate errors during data write cycles, such that subsequent reads of the corrupted addre...

RTC Initialization Issue

Posted on November 12, 2015 at 14:29Hi CommunityI have an issue with the Real Time Clock of the SPC560D. My application try to read the RTC.RTCCNT register. Every time during the read process the program pointer goes to 0x0000000E0, therefor it poin...

SPC560D - power control modes

Posted on June 30, 2015 at 16:50Hello,I am using standby mode for SPC560D MCU. The datasheet mentions about using DRUN or software reset for exiting this mode. Can you please explain on,1. How to configure the DRUN mode? I tried using API 'halSPCSet...

ssk by Associate II
  • 4516 Views
  • 61 replies
  • 0 kudos

SPC560B60, SPC560B64 and ''Freescale SPC5607B'' compatibility

Posted on December 07, 2015 at 12:46Good morning, I've 2 questions: First, I'm wandering about the differences between: the SPS560B60 and the SPS560B64? Are they compatible in the sense that the same code would run the same in both devices? (I'm alr...

mbahtat by Associate
  • 430 Views
  • 1 replies
  • 0 kudos

using UART

Posted on November 27, 2015 at 11:13Hello everybody, I'm using the SPC56EL70L5DISP board.In order to use UART, I put the jumpers in J18 and J20 to connect UART-MCU LIN0, following the board user guide.Running the test example with UART and blinking ...

eDMA with SPC560B

Posted on November 30, 2015 at 16:05Hi all, I try to get the eDMA Modul working. My starting point is an example code from the document ''Qorivva Simple Cookbook “Hello World�? Programs to Exercise Common Features on MPC5500 & MPC5600 Microcontrolle...

dominik2 by Associate II
  • 630 Views
  • 2 replies
  • 0 kudos

Using SRAM

Posted on October 30, 2015 at 12:43I am using SPC560D with SPC5Studio. I want to save the device configuration/status before putting the device to standby mode and use/retrieve this status when the device exits standby mode. Can this be achieved by ...

ssk by Associate II
  • 864 Views
  • 6 replies
  • 0 kudos

SPC5Studio 3.7.1 is available !!!

Posted on November 24, 2015 at 10:24Dear All , SPC5Studio 3.7.1 is available *** Highlights *** - Documentation Update (Pinmap, ClockTree, SPC5Studio userguides) - Several bugs and improvements, please refer to https://my.st.com/public/STe2ecommuni...

eMIOS overflow callback and frequency range

Posted on October 19, 2015 at 12:20Hello, when I was working on SPC56EL with older SPC5 Studio versions, the overflow callback was called only when the internal counter was overflowing. This was perfect to detect too low frequency which can't be mea...

Updates

Posted on November 10, 2015 at 15:44Hello everybody,I tried to update SPC5 studio but i got the error ''No repository found containing:''on every update package.Trying to fix this problem I accidentally erased repositories.Now i need to know what si...