SRAM faut injection
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-11 2:31 AM
Hello everybody,
I'm working on the SPC56EL70L5 From the reference manual, I know that:“For platform RAM, the intent is to generate errors during data write cycles, such that subsequent reads of the corrupted address locations generate ECC events, either single-bit corrections or double-bit non-correctable errors that are terminated with an error response.�?
So, I coded (I put the related assembly too):
SPP_MCM.ECR.R=0x33; \\to activate reportings
0x00001D7E: 70 1F E7 F4 E_LIS R0,0xFFF4
0x00001D82: 4B 37 SE_LI R7,0x33
0x00001D84: 01 06 SE_MR R6,R0
0x00001D86: 34 E6 00 43 E_STB R7,0x43(R6)
SPP_MCM.EEGR.B.FR11BI=1; \\ injection
0x00001D8A: 70 FF E7 F4 E_LIS R7,0xFFF4
0x00001D8E: 50 07 00 48 E_LWZ R0,0x48(R7)
0x00001D92: 48 16 SE_LI R6,0x1
0x00001D94: 74 C0 64 E6 E_RLWIMI R0,R6,0xC,0x13,0x13
0x00001D98: 54 07 00 48 E_STW R0,0x48(R7)
But, execution of instruction at 0x00001D8E causes hangs in
_unhandled_exception:0x000003A0: 78 00 00 00 E_B _unhandled_exception (0x000003A0))
This is not the expected behavior, what is going wrong?
Thanks in advance for the help- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-14 6:45 AM
Hello Stefano ,
It is linked to the compiler optimization. to set a bitfield is not recommended in some compilers. I recommend to use the register directly :// Force RAM One 1-bit Data Inversion
#define ECSM_EEGR_FR11BI_MASK 0x1000
/* Force internal SRAM one 1-bit correctable data error */
SPP_MCM.EEGR.R = (uint16_t)(ECSM_EEGR_FR11BI_MASK | 0);
Best regards
Erwan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-16 3:40 AM
Thank you, it worked.
Best Regards