Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC570S40 start in RUN0 mode with debugger

Posted on February 05, 2018 at 14:39Hi ,I'm new and I 'm developing on SPC570S40E1.I've a demo board and my final target board.When I try to debug my application I've 2 different behavior between  demo board and final target: on demo board during cl...

Safety SIL application and toolchain with SPC570S50E1

Posted on February 01, 2018 at 15:26Hello to everybody.I'm doing a research about different microcontrollers suitable for safety application, SPC570S50E1 is a very interesting candidate.The discussion is about what kind of support can I have for thi...

CFlash module example code for SPC560B60L7

Posted on January 31, 2018 at 01:17Hello!I'd like to use CFlash module without using C90LC Standard Software Driver(SSD).But I don't konw how to configure it.Could you provide me an example code?i.e) CFlash initialize, CFlash Erase, CFlash Write, et...

Hank Im by Associate II
  • 569 Views
  • 2 replies
  • 0 kudos

Resolved! Illegal instructions when using -fpic

Posted on December 22, 2017 at 09:55 Hello, I'm trying to make my application position independent so that I canplace the software anywhere in the flash of the SPC564B I'm using. Is this possible using the free FreeGCC v4.9.3 with VLE suppo...

Resolved! SPCSetRunMode not return ......

Posted on April 13, 2017 at 10:27 SPCSetRunMode not return ...... board: Discovery Plus Kit for SPC56 L line - with SPC56EL70L5 MCU my step: file->new sp5 studio Application wizard-> select Discovery Plus Kit for SPC56 L line - with SPC56E...

0690X00000606PiQAI.png 0690X00000606kdQAA.png 0690X00000606kxQAA.png 0690X00000606l2QAA.png

Resolved! Training/Tutorial about SPC5Studio

Posted on January 17, 2018 at 17:23Hi, I'm a new starter with ST MCU.Are there training/tutorial about SPC5Studio?Many thanks,Roberto#spc5studio #training #tutorial

Resolved! Phase-Shift PWM Modulator SPC5x

Posted on January 16, 2018 at 15:39Hi folks,I'm a new starter here, is there a section with code example, training, etc?Currently, I'm working on the control of a power electronic converter with a phase-shift PWM modulator.Thanks for any help or adv...

Resolved! SPC5Studio build failure, too

Posted on January 15, 2018 at 18:20My problems same as https://community.st.com/message/10560 The SPC5Studion was upgraded to 5.7.1But I selected SPC56-DISCOVERY(BOARD) , DRIVERS --STM My toolchains is the GNU make builder of spc5studio default.Keep...

Resolved! SPC5Studio MarketplaceDiscoveryStrategy failed

Posted on January 10, 2018 at 12:38Hello,I have a very similar problem to that asked by https://community.st.com/people/71687 on May 3, 2016. I have just installed SPC5Studio 5.7.1 and am attempting to use the Eclipse Marketplace to download the Pow...