Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

download.spc5studio.com

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/New or updated componentsRLA 1.12.0   SPC58ECxx : Machine check demo application   SPC58xHxx : OctalSPI driverNetwork 1.8.0New netwo...

Resolved! canbus transmission

I'm using the demo board SPC560P - DISP and the example SPC560Pxx_RLA CAN Test Application for Discovery .This Test Application use the CAN loopback, if I remove the flag of FlexCAN Enable Loopback in the can configuration setting I'm expecting to se...

gp73 by Associate III
  • 582 Views
  • 2 replies
  • 0 kudos

Resolved! __attribute__ ((aligned (32))) doesn't work.

i'm working with spc570s and using gnu free gccc in spc5studio.In my program I need to apply __attribute__(( aligned(32))) to an const struct variable.I tried like this but it does't work.for example.typedef struct{uint32_t aa;uint 32_ bb;...}Astatic...

HIm by Associate II
  • 3107 Views
  • 8 replies
  • 0 kudos

How to produce single pulse alone using eTimers?

I cant able to produce by the below configurations asCTRL1->ONCE=0UCTRL1->LENGTH=0UCCCTRL->CMPMODE=0UCTRL2->OUTMODE=8UCTRL1->CNTMODE=1Uand also by various combinationsthe most important thing is that i want to produce a single pulse by having control...

PE.1 by Associate
  • 228 Views
  • 0 replies
  • 0 kudos