Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC58EC with CAN BUS and UART

Hello dear Engineers.I am using SPC58EC Dev. board and want to use CAN BUS and UART in the same time. I can send Enter command from my keyboard to SPC58EC board via USB to TTL module (TX RX pins). But how can i do that, when i press enter it can send...

Nurlan13 by Associate
  • 430 Views
  • 0 replies
  • 0 kudos

Running code without debugging (SR5E1-EVBE7000P)

Hello,I'm trying out examples for the SR5E1-EVBE7000P development board. I use StellarLINK to implement the code on the flash and when I run it via RESUME the code runs. But if I execute Terminate and want to run the code without StellarLINK, e.g. by...

What does "Enable All Peripherals" in AN3324 mean?

The Application note AN3324 (Implementing power-on self tests for SPC56EL60 in locked step) says in Figure 2 (page 9) that one should "Enable All Peripherals" before initializing the FCCU. What does "enable" mean in this context? Does it mean setting...

DaveJ by Associate II
  • 398 Views
  • 0 replies
  • 0 kudos

spc58 jtag/Nexus

I through Nexus to read/write memory.Is the response correct?The steps to enter Nexus from jtag are as follows:1. TDI: Shift-IR(0x01) Shift-DR(0x00000000) TDO: 0x11140041it confirms the jtag id is correct2. TDI: Shift-IR(0x2A)it through jtag to enabl...

and_w_0-1732692150611.png
and_w by Associate
  • 411 Views
  • 0 replies
  • 0 kudos

spc582b register

Is the  base address  of Flash user registers  0xF7FE0000. In rm0403,I don't seem to have found any other relevant addresses。 

and_w_0-1732671029472.png
and_w by Associate
  • 335 Views
  • 0 replies
  • 0 kudos

MCU SPC58

Hi anyone could help me how to read this ecu infineon micro using bootmode?oR HOW TO READ THIS FLASH MEMORY

image_67511809 (1).JPG image_67239681.JPG

Resolved! SPC5 Studio

Hello, I am Erdem.I am an R&D engineer at Devimsel Elektronik. I will use the SPC560P processor on my own PCB board. For this I need instructions for using SPC5 studio. How do I make configurations such as pin and clock tree? Can I get an instruction...

Eakso.1 by Associate II
  • 2559 Views
  • 6 replies
  • 1 kudos

Resolved! EV-VN9D30Q100F for SPC582B-DIS or SPC58EC-DIS GUI firmware

Hi,i need some help for the EV-VN9D30Q100F. It says there is a dedicated Software for the SPC582B-DIS or /EV but i can't find it nowhere. The board connects to the GUI (STSW-EV-M09SPI), so far so good, but without the firmware on the MCU, i can't tes...

PNeub.2 by Associate II
  • 664 Views
  • 1 replies
  • 1 kudos