Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5CX Histogram Data at Low Frame Rate?

I read in other posts that it is not possible to read out the VL53L5CX histogram data because there is just too much of it. But I was wondering if it is possible to read it out if we do not care about real-time operation and are okay reading out the ...

FGuti.2 by Associate II
  • 2712 Views
  • 5 replies
  • 0 kudos

Anyone using VD6283 without stmcube ?

Hi everybody, I'm trying to interface vd6283 (I own vd6283-satel breakout board) with other non-stm32 microcontrollers (esp32, samd21, ecc) .stm's library (x-cube-als) claims that "should" be easy porting on another hw but...it's not that easy....Did...

MZ68 by Associate II
  • 1137 Views
  • 1 replies
  • 0 kudos

Is there an ACTUAL datasheet for the VD6283 available?

Having been using ST sensors for decades, this is the first time I stumble onto this perplexing problem: there is no datasheet available!There is a .pdf called 'datasheet', but it only documents half the registers and them very superficially. There i...

KPalo.2 by Associate
  • 1288 Views
  • 1 replies
  • 0 kudos

VD6283 Sensing problem with range?

I have been using VD6283 with STM32 and have found that they work well in detecting flicker when the light source is near the sensor. However, I have encountered an issue where the flicker is not detected when I move away from the light source.Additi...

MKash.3 by Associate
  • 1460 Views
  • 1 replies
  • 1 kudos

VL53L4CD cover glas specification

I am using the VL53L4CD for my current project and I would like to add acrylic glas cover to it. I am actually using 4 of the ToF Sensors and would like to cover all of them with one glas.What type of glas can be used here, are there any known limits...

DrD00m by Associate III
  • 2067 Views
  • 2 replies
  • 1 kudos

VL53L4CD using characterization GUI Tool

Hi,I purchased the P-NULCEO-53L4A1 package and am testing it to use Liquid Level Monitoring.I have downloaded STSW-IMG039 and am referencing AN5851 and STSW-IMG039-L4CD.pdf.I used the provided GUI Tool (GUILiquidLevel.exe) for Nonliearity correction....

LJinH1_0-1691033942833.png LJinH1_1-1691033948232.png LJinH1_2-1691034240182.png LJinH1_3-1691034551871.png
LJinH.1 by Associate II
  • 2839 Views
  • 5 replies
  • 3 kudos