Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Intrinsic matrix of VL53L8CH/X

Hi there, I have recently met a problem in calibration of VL53L8CH/X. So I need to get its intrinsic matrix. Where can I find it?

Bryce by Associate II
  • 1737 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L5CX not measuring far distances

I am using multiple VL53L5CX sensors to measure distances around a robot using the 4x4 resolution, target order closest and ranging in countinuous mode. When I'm measuring a distance close to the sensor ~500mm and then the object is suddenly removed ...

mreumer by Associate
  • 2390 Views
  • 2 replies
  • 1 kudos

water level monitor with time of flight sensor

Hi friends,  currently Iam working for the project (water level monitor with time of flight sensor).  For my application it should sense  around 4 meters.  I have selected the sensor (vl53l5cx) which is 2.7 meters sensing range which black reflective...

Arun by Associate
  • 1488 Views
  • 1 replies
  • 0 kudos

Resolved! About temperature calibration of VL53L1X

Hello,I am developing a system using VL53L1X.I have read UM2510 (A guide to using the VL53L1X ultra lite driver).This library implements the function called "StartTemperatureUpdate".The description for this function states, "This function performs th...

KArai.2 by Associate II
  • 3152 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L4CX long series of bad measures

Hi, I'm testing some VL53L4CX for about 10 months with nrf52832 using I2C. It's used in very dark conditions and within 3m and I take 15 measures 24 times a day.Between periods of measures I completely power off the sensor with an LDO.It works fine f...

about argument of VL53L1X_CalibrateXtalk()

Dear Sir,There is a question about argument  VL53L1X_CalibrateXtalk().For cross talk calibration, we will use  VL53L1X_CalibrateXtalk()  with argument of uint16_t TargetDistInMm,we should give Xtalk calibration distance to  the argument. But, we wond...

DSai.1 by Associate III
  • 1504 Views
  • 1 replies
  • 0 kudos

Resolved! Looking for a Distance calculating Sensor

Hi ,we are looking for a distance sensor that meets the below requirements1.Working distance 5mm to 200mm2. Resolution steps: 0.01mm steps what is the minimum resolution steps your sensor can provide. Let me know if you need anything else. 

Resolved! I2C address problem with SATEL-VL53L7CX

Hello everyone,I am trying to read the distance data from a VL53L7CX ToF sensor with a Teensy 4.1 board. I am using the SATEL-VL53L7CX breakout board. The sensor is detected by the Teensy, however I when I try to check if the new data are ready to be...

Resolved! VL53L5CX VL53L5CX_ResultsData distance_mm mapping

Hello,Been thru all the specs I can find on the VL53L5CX but I can't find how the Zones numbers map to array of distance_mm in the VL53L5CX_ResultsData  struct.Is Zone 0,0  distance_mm[0] please?Or can someone point me to the spec/page please?Many th...

Iknig.1 by Associate II
  • 1568 Views
  • 1 replies
  • 0 kudos