cancel
Showing results for 
Search instead for 
Did you mean: 

Do all VL53L* sensors use the same VCSEL with the same power?

FGuti.2
Associate II

I was wondering if all the VL53L* sensors use the same VCSEL illumination source with the same average and peak power. I would think the the long-range sensors (VL53L1CB) and the sensors with wide FoVs of 63 degrees, would need a more powerful VCSEL.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Anne BIGOT
ST Employee

There are not using the same VCSEL illumination source as it impacts the different features reached.

So ST is using a set of different VCSEL.


Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised.

ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'