Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VD55H1 release date?

Hi! Is there release date for the new VD55H1 sensor? Does it come with a development set?Best,Wayne

DWang.7 by Associate III
  • 1559 Views
  • 1 replies
  • 0 kudos

VL53L7CX - Can it detect glass walls?

Hello,I was unsure if the VL53L7CX would be able to detect glass walls. Often ToF sensors are unable to as light passes through the glass, but was curious that the non-zero reflectance of glass (usually <10% but still nonzero) allows VL53L7CX to dete...

Resolved! VL53L4CX one-cycle delay in the returned data

Hi:When I move the object detected by the VL53L4CX, I find that there is a one cycle delay in the distance it returns. Is this because its first data is discarded?(Range status=6)? Is there a way to improve this?Thankyou.Cyt 

sctz by Associate III
  • 1587 Views
  • 2 replies
  • 0 kudos

Vl53l1x ToF Sensor does not initialize

Hi,I use to 12 ToF(Vl53l1x) sensor on the robot for security range detect. And at the some situations, this sensors stop ranging data. I detect last regular data and then reset sensor. when starting sensor can do bootstate function. But can not do se...

hsynklc by Associate II
  • 1885 Views
  • 1 replies
  • 0 kudos

Resolved! distance measurement

Hello I want to measure the distance of water in a cylindrical container to the lid of the cylindrical container. I need to find the height of the water by subtracting the measured distance from the height of the cylindrical container. Since there is...

AKULC.1 by Associate II
  • 2916 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L5CX & VL53L1CB resolution

Hello,I can't find the measurement accuracy of the 2 sensors mentioned above in your documentation. Could you please provide me with this information?Thank you.Regards, 

Florian3 by Associate
  • 2141 Views
  • 1 replies
  • 0 kudos

Difference Between A and B Message

I've seen references to various A and B or (even and odd) messages for the ToF sensors.In my application, it turns out that every other measurement is not great, so if I throw out packets based on their message ID count, then I get perfect data but a...

Resolved! VL53L5CX safety for human detection

Hello,I plan to use VL53L5CX to measure the distance between the robot and the user (human) in the walker project. I would like to ask if it is safe or not. Regards,Fehmi.

FKara.3 by Senior
  • 1706 Views
  • 1 replies
  • 0 kudos

Resolved! Device unique ID for VL53L5CX ?

Hello all,does the vl53l5cx ULD API (STSW-IMG023) can expose  a unique device ID for the VL53L5CX ? Something similar to the VL51L1 API function call "VL53L1_Error VL53L1_GetUID(VL53L1_DEV Dev, uint64_t *pUid)"  in the driver SWSW-IMG019 ? Kind regar...

LK by Associate II
  • 3224 Views
  • 6 replies
  • 1 kudos