Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Device unique ID for VL53L5CX ?

Hello all,does the vl53l5cx ULD API (STSW-IMG023) can expose  a unique device ID for the VL53L5CX ? Something similar to the VL51L1 API function call "VL53L1_Error VL53L1_GetUID(VL53L1_DEV Dev, uint64_t *pUid)"  in the driver SWSW-IMG019 ? Kind regar...

LK by Associate II
  • 3255 Views
  • 6 replies
  • 1 kudos

Resolved! Cover Glass - XTalk Limit (Algorithmn) for various FlightSense Products

Hi all,I'am wondernig about the max XTalk level in kcps which various FlightSense products can compensate. I found only for the new VL53L8CX Sensor a  xtalk compensation limit of 300 kcps - mentioned in application note  AN5939 in section 7 : Guideli...

LK by Associate II
  • 2529 Views
  • 3 replies
  • 2 kudos

Resolved! Gesture Library for VL53L5 linking error for b-u585i-iot02a board: undefined reference to taylor_sqr

Hello to all, I create a new project using STM32CubeMX for the b-u585i-iot02a board. Then I added to the project the software and the library for the gesture recognition STSW-IMG035, specific to M33 processor. Compiling, I have this error:Description...

clemente by Associate III
  • 4018 Views
  • 3 replies
  • 1 kudos

IR080C0-IC09-A066-2 cover window for VL53L1X

I am using cover glass window IR080C0-IC09-A066-2. I want the design to be IP69. Where I can get the information that the cover glass can withstand If it is subjected to high water pressure (10000 kPa) and high temperature(80*C)?

Ali_SE by Associate
  • 2231 Views
  • 1 replies
  • 0 kudos

VD6283 on Arduino UNO

Hello everyone,i bought the X-Nucleo-6283A1 development Board from ST together with an Nucleo-F401RE Developmentboard.I have also installed the GUI and it works ok, the calculation of CCT is not performing correct, but thats ok so far...Now i wanted ...

SBurc.1 by Associate II
  • 3674 Views
  • 6 replies
  • 0 kudos

VL53LX API Compatibility

I ended up accidentally discovering that the VL53LX API is compatible with two different sensors.I'm using this platform implementation for Linuxhttps://github.com/ned14/VL53L3CX_rasppiI have the VL53L3CX but also the VL53L4CD.  I've seen that the VL...

ToF VL53L4CD load capacitance calculation

Hi, I am struggling to understand how to calculate the load capacitance when adding the pull-up resistors in my circuit with VL53L4CD ToF sensor to run the sensor in fast mode plus. The datasheet states that:Suggested pull-up and series resistors for...

Gabor23 by Associate II
  • 2234 Views
  • 3 replies
  • 0 kudos

Reading several VL53L7CX sensors with a Nucleo

Hello everyone,I am trying to read data from three SATEL-VL53L7CX, using only their mini-PCB part, with a Nucleo F401RE.To do so, I did the following wiring:each sensor is using a different I2C bus (sensor 1 is plugged on SDA1/SCL1, sensor 2 on SDA2/...

VL53L7CH, VL53L8CH with AI

As it is described both models are dedicated for  AI applications. Where can I find examples of usage or materials to start?I assume I can use NEAI Studio?

KNawa.1 by Associate II
  • 2015 Views
  • 3 replies
  • 0 kudos