cancel
Showing results for 
Search instead for 
Did you mean: 

When VL53L5CX Time-of-Flight sensor is in threshold detect mode, will it trigger only on what would be a Status 5 valid range measurement?

DBonh.1
Associate III

When VL53L5CX Time-of-Flight sensor is in threshold detect mode, will it trigger only on what would be a Status 5 valid distance? Thanks! -Doug

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

There are a few different statuses that are assumed to be 'good'.

They are:

·         5 – RANGE COMPLETE                ​

·         6 – RANGE COMPLETE_NO_WRAP_CHECK   ​

·         9 – RANGE COMPLETE MERGED PULSE    ​

·         12 – TARGET DUE TO BLUR  

6 only happens on the first range.

9 means there might be a couple of targets that are merged together

12 means the target might be do to a target in an adjacent zone.

But basically your are correct.

  • john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

2 REPLIES 2
John E KVAM
ST Employee

There are a few different statuses that are assumed to be 'good'.

They are:

·         5 – RANGE COMPLETE                ​

·         6 – RANGE COMPLETE_NO_WRAP_CHECK   ​

·         9 – RANGE COMPLETE MERGED PULSE    ​

·         12 – TARGET DUE TO BLUR  

6 only happens on the first range.

9 means there might be a couple of targets that are merged together

12 means the target might be do to a target in an adjacent zone.

But basically your are correct.

  • john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
DBonh.1
Associate III

Gold! Thanks John!