Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X inaccurate off-perpendicular?

I'm using the VL35L0X.ino demo code on an Arduino UNO and a clone VL53L0X sensor. I very carefully measured the off-perpendicular distance measurements obtained from the VL53L0X and compared them to actual tape measure measurements. On average there...

0693W000001cY9MQAU.jpg 0693W000001cY9RQAU.jpg
FPayn.1 by Associate III
  • 3373 Views
  • 6 replies
  • 0 kudos

Resolved! VL53L5CX status Mean

when I use VL53L5CX and get a status, then check with the table, but I still need further description than can explain STATUS means what.It's better like the picture below. Now I meet status 2, but I do not know why this happened.  

MasterNi_0-1700107393838.png MasterNi_1-1700107734675.png
MasterNi by Associate
  • 2302 Views
  • 1 replies
  • 0 kudos

Resolved! Long Range TOF

Hello, I want to ask about the maximum range of VL53L1CB, as it says in the table (as seen in attached photo) that it's up to 8m. However, in data sheet or specification just says over 400cm.1) So is the performance should be good at 8m range outdoor...

Screenshot 2023-11-16 at 10.26.20.png
E_K by Associate
  • 2535 Views
  • 1 replies
  • 0 kudos

VL53L5CX ULD vl53l5cx_check_data_ready() returns error CA 81

I'm trying to implement the VL53L5CX ULD v1.3.4 on an Atmel ATSAM4L. Per an Total Phase I2C analyzer, I have it almost all running correctly. It's uploading the firmware, and the firmware bytes captured by the I2C analyzer match the bytes in vl53l5cx...

DBonh.1 by Associate III
  • 7441 Views
  • 8 replies
  • 0 kudos

Resolved! VL53L4CX not NewDataReady

Hello, i've been using a couple of VL53L4CX tof for a month with no problem so far, but recently i bought a few more and none of these work. (These new ones are the same model that the ones that worked).Analyzing with a digital osciloscope the I2C co...

JaFrauca by Associate
  • 3513 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L5CX sunlight range

Please tell me the brightness range of sunlight that VL53L5CX can be used with.

Taro by Associate
  • 2314 Views
  • 2 replies
  • 0 kudos

Resolved! User Manual for STSW-IMG035

Howdy,I am working on a project that utilizes a VL53L5CX ToF Sensor, and I am looking to use the STSW-IMG035 libraries for M0+ chips in my project. In the databrief for the sensor, it refers to "an easy-to-read user manual" which I cannot seem to fin...

adirt by Associate
  • 1453 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to start ranging on the vl53l8cx

Hello,I've already used the vl53l5cx and it worked flawlessly, so I decided to try the newest one. I'm working on an esp32s3 and a satel-vl53l8 using the ULD. I completed the platform file, and it initialized the sensor without errors. But when the s...

RJRP by Associate II
  • 3610 Views
  • 3 replies
  • 0 kudos

Resolved! Explanation of VL53L0X_GetRangingMeasurementData() output

Hi,We are currently in a project where we want to use the VL53L0X chip for ranging. And the example code with PC application seems to work quite good. the next step is to create a PoC using our own system (where we are now).I am currently reading up ...

RBerk.1 by Associate III
  • 17354 Views
  • 8 replies
  • 1 kudos

Resolved! Using VL53L1X to get an ambient light value

Hi,in my next application I plan to use VL53L1X. What I also need, independent from the object detection, is the amount of ambient light. Would it be possible to read that value from VL53L1X using it's full API? Is that value at all available in one ...

PaKw by Associate
  • 1920 Views
  • 1 replies
  • 1 kudos