User Activity

Hello @John E KVAM ,Table 14 in the datasheet shows power consumption in Autonomous as going as low as 4.5 mW, but is this only the AVDD power? or total device power? Because I do measure low power draw at those levels, but only on the AVDD pin (and ...
The eval board for the VL53L5 has a GUI that displays all of the zones. Is there a similar GUI for the 53L8 eval board? I don't see one listed on the Tools and Software tab for the eval board. Or is there a way to make the L5
When VL53L5CX Time-of-Flight sensor is in threshold detect mode, will it trigger only on what would be a Status 5 valid distance? Thanks! -Doug
I'm looking at the I2C spew from a VL53L5C, and it appears to be values for each of 64 zones. Data for a particular zone starts with Z_______ where the blank is the zone number. But instead of starting with Z 0 to Z3F (0 to 64) it goes from ZFFFFFFC ...
I'm trying to implement the VL53L5CX ULD v1.3.4 on an Atmel ATSAM4L. Per an Total Phase I2C analyzer, I have it almost all running correctly. It's uploading the firmware, and the firmware bytes captured by the I2C analyzer match the bytes in vl53l5cx...
Kudos from
Kudos given to