Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TOF sensor distinguishing between object and person

Hi all,I'm working on a product that uses a TOF sensor (exact type# TBD) to identify if someone(s face) who is sitting in a chair is present within a certain distance and angle (around 20 degrees). If the right conditions are met the product should b...

TH3 by Associate II
  • 3757 Views
  • 6 replies
  • 1 kudos

Resolved! Vl6180x cross-talk calibration procedure

I am currently trying to perform the Cross-talk calibration procedure, but I am confused because the procedures mentioned in the documents "Proximity and ambient light sensing (ALS) module" and "VL6180X cross talk compensation implementation" are som...

Andy_Chien_0-1721576321533.png Andy_Chien_1-1721576504341.png

Resolved! vl53l0/1xv2 interface to 3rd-party MCU/MPU

hi anyone can please help me for the integrating vl53l0 sensor with rx71m mcu,because i am not getting specific document for communicating it with rx71m over i2c please support

Mak by Associate
  • 1514 Views
  • 1 replies
  • 1 kudos

Resolved! Vl53L5/VL53L7 temperature reading

Hi,i am using both the VL53L5 and L7 in a quite limited space, where the sensor need to run in the 8x8 continuous mode. Therefore, the thermal design is quite challenging.  So, my question is: what temperature does the sensor specifically deliver wit...

lukaskn by Associate II
  • 2304 Views
  • 2 replies
  • 1 kudos

Resolved! vl53l5cx_set_VHV_repeat_count not found

In the guide to using the VL53L5CX multizone Time-of-Flight ranging sensor it's described that for periodic temperature compensation the function vl53l5cx_set_VHV_repeat_count has to be called.I can't find the function in any header or c file.

PBoer.1 by Associate II
  • 1215 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L5/L7CX target status validity

Hello,the VL53L5CX and L7CX ULD guides mention that a target status of 6 and 9 should be considered with a confidence of 50 %, while a comment in the api.h file says that  "5 & 9 means ranging OK", which gives the impression of a higher confidence ra...

lukaskn by Associate II
  • 1615 Views
  • 1 replies
  • 0 kudos

Resolved! How exactly do I read the histogram on VL53L8CH

Hello Community, I am new here and new to this field as well. I am currently using the VL53L8CH Lidar Sensor which has a MZAI some GUI tool to access and save data logs along with some visualizations of the data.I am currently doing some experimentat...

koch by Associate II
  • 2552 Views
  • 2 replies
  • 1 kudos

Resolved! Calibration card

Calibration of ToF sensors requires a target which is '17% reflective'. Can I take it this means a simple peice of paper or card printed on a laser printer at 83% black (greyscale)?Thanks

Resolved! Wait for sensor booted fails

I was using the sensor until now on an Raspberry Pi with direct access to the I2C bus without problems.Now I use an FT260 USB-I2C interface to communicate to the sensor from a PC via USB. In principle the communication is working, e.g. vl53l5cx_is_al...

PBoer.1 by Associate II
  • 2687 Views
  • 4 replies
  • 0 kudos