Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TOF Sensor Lens Fogging and Icing Problems

Hi all.I'm using a TOF sensor VL53L0X to make a small short range probe. the TOF sensor is not suitable for direct exposure, so there will be a piece of lens to cover the TOF sensor. Now the problem is, in the low-temperature environment, the lens su...

Resolved! VL53L7CX Driver - Implement from VL53L5CX driver?

Hi, I have implemented the VL53L5CX driver for a Nordic controller, and it works fine. Now, I want to implement the VL53L7CX driver for the same Nordic controller. Can I use the VL53L5CX driver as is, or will I need to make changes? Additionally, are...

Resolved! VL53L1X using with another laser source

Hi, I had a query regarding the VL53L0X TOF sensor. Is it possible to block the laser on the board and use an off board laser of same wavelength and get readings from TOF sensor? such as intensity readings only?   

vishnusf by Associate III
  • 1740 Views
  • 2 replies
  • 1 kudos

Resolved! Extracting distance data from VL53L8CH --> CNH histogram data

Hello Community,I had a doubt and wanted an explanation to it relating to a document published by STM electronics, https://www.st.com/resource/en/application_presentation/26oct2023-artificial-intelligence-enabler-time-of-flight-sensors-with-cnh-data....

koch by Associate II
  • 3912 Views
  • 2 replies
  • 1 kudos

Integration of multiple VL53L0X

Dear ST,I am looking for a solution with the integration of multiple ToFs such as VL53L0xObjective: 1. Find the distance between the ToF_x(emission only) and ToF_master(reception only)As the reception zone of vl53l0x is 25 degrees , either one or mul...

Capt_Jac by Associate
  • 2401 Views
  • 2 replies
  • 0 kudos

VL53L8CX SATEL use with Arduino Or ESP32?

Does anyone know if the VL53L8CX SATEL can be used with an Arduino board (just for testing)? Or ESP32? I've tried the basic wiring I have done for other breakouts, but it doesn't work. If so, please share how it should be wired. Also, I have used ver...

MCham.8 by Associate
  • 4852 Views
  • 5 replies
  • 4 kudos