Hello We are planning to work on STM32MP2x processors in our custom design boards. We tried with latest version of CUBEMX for pinmux but it's not available. So, we would like to ...
Hello, I create new STM32 project for STM32MP131AAG3 with baremetal. I encounter the following errors when to build the codes of DMA generated by STM32CubeMX. undefined reference ...
Hello, I am trying to create a new STM32 baremetal project for STM32MP131Axx. Errors occurred when to build the project that ADC2 is enabled by using STM32CubeMX. 'ADC1' undeclared...
Select a new prject in CibeMX this case STM32Mp157AAA ) Select PZ1 and PZ2 pin. Configure Pz1 output assign PZ2 for EXT IN and assign to Cortex M4 Generate MX output file Issue 1: No GPIO pin...
STM32MP157AAA custom board with DRAM, SD- EMMC, USB and UART , Discrete power( no PMIC) . The board uses discrete oscillators for HSE and RTC, so they are set as Crystal OSC for both in...
I am trying to configure some HW IP to work with the M4 core of the STM32MP157, I can find only the GPIO already assigned to other IPs ont he development Kit. How to configure GPIO's and configure i...
We are using the STM32MP157AABx device in our project and updating to the v5.0 Ecosystem and STM32CubeMX v6.9.0. When we generate our device tree files, the optee-os device tree tries to include: #...
I've been trying for hours to read an analog value from a pin and write it over UART with no success on my STM32MP1. I've assigned PF14 to ADC2_INN2 and set IN2 to "IN2 Differential", then I generate...
Hello all, I am used to the regular MCUs STM32Fx families where I'm used that the main.h has all the #defines of the GPIOs and other peripherals. I'm now using STM32MP1 generating code for CM4 and ...