STM32CubeMX (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 identify CM4/CA7 assigned periperhals

Hello,with CubeMx 6.9.2 i am generating Code for CubeIDE with the goal to figure out which periphery is assigned to the CA7 or the CM4.With Freemarker it is possible to get information about which IP's are assigned and used but i have no idea how to ...

Jagr by Associate II
  • 49 Views
  • 0 replies
  • 0 kudos

I used STM32CubeMX version 6.3.0 thinking it was the correct version for Ecosystem 3.0 just to discover I should have used STM32CubeMX version 6.2.1. Is there a way to move my projects backwards?

I have several projects already configured for STM32MP157C and I don't want to have to build them all over again if I can help it. Also, my team is asking I not move the Ecosystem (but if that is my only answer I will.)

SLetter by Associate III
  • 244 Views
  • 2 replies
  • 1 kudos

STM32MP135

I would like to Design STM32MP135FA Processor based data logging and file accessing throgh Ethernet Kinldy suggest below application possible in STM32MP135 series Processor.1. Two ethernet going to use - One for SD card file acess / another one for F...

JMari.11 by Associate
  • 234 Views
  • 0 replies
  • 0 kudos