I am trying to make a precise delayed pulse for my project that does not use interrupts. I plant to use TIM1 or TIM8 on a STM32H7A3 using the TI2FP2 input to trigger and reset the counter in one-puls...
hello guys, i am using a FTDI FT232B17 for serial communicaiton with my stm32f429 board. i'm using keil uvision, and not using any libraries other than stm32f429xx.h to write the code. i am fa...
Hello STM32 community, I'm encountering an issue with my STM32L562VET controller where the debugger gets stuck at the `HAL_GetTick()` function. When debugging, the program seems to halt at this poin...
Hello ST Community, I'm encountering difficulties while attempting to connect and debug my STM32 microcontroller, and I'm seeking guidance from the community. I have erased the full chip flash ...
Hi everyone, I'm using a STWINBX1. Some documentation say that RTC can be plug to Vbat. In my case, my board won't be plug to current and will only work with a battery. My question is simp...
Hello All, I bought the NUCLEO-F446ZE board and would like to use Ethernet port but it is not soldered onto the board. Which RJ45 jack do I need to buy? Could someone provide reference to Mous...
Hello, I'd kindly ask for some help on determining exactly which MCU pin is connected to STMod+ extension board. Which pins exactly are connected to STMod+ pins 2 and 3 ? It seems like two choices...
...From my actual understanding, this means that the COM Port is not active because SB4 and SB7 are "ON" too? Is this correct? If this is true and I have to set SB4/SB7 off. How do I set SB4 a...
I am having a nightmare trying to install a nucleo F412ZG (https://www.st.com/en/evaluation-tools/nucleo-f412zg.html) under windows 11 64bits. It has an onboard ST-Link V2-1. In the device manager ...