I want to read the serial output from the STM32 F405 Feather using the SWV on Cube Programmer, but I do not receive Serial output from the board. I am running the .hex file from this Arduino sketch o...
Hi, I'm going to say that this is a really nooby question, however I cannot find the answer anywhere. Background, I'm using a nucleo F103RB, and I've programmed it using CubeIDE. I can connect the ...
We are working with the STM32H745I-DISCO and a custom daughter board we designed that interfaces with the Arduino Style Connectors on the DISCO Board. We believe that there are errors on b...
Hi Community, I have recently purchased Nucleo H7A3ZI board and while trying to connect through Stm Cube Programmer i have found that it is not detecting target itself. What is possible reas...
Dear ST-Electronics Community, I hope this message finds you well. I've noticed a limited number of posts (1 or 2) regarding the import of Altium format files and the subsequent development of custo...
I have a problem in my project involving the STM32L010RB MCU and the HC05 Bluetooth module. Currently, the system operates smoothly when connected to the USB port. The HC05 Bluetooth module successf...
Hi Guys I'm Trying to find stm32l073rz Nucleo board datasheet that contains the boards pin description, but I can't find it anywhere I have found those but when I compare the pin description ...
I am trying to bring up the STM32U5A9J-DK wherein I can use the external NOR_FLASH over OctoSPI_1 and the external PSRAM over HSPI_1 -- both in memory mapped mode. I am trying to use the STM32CubeMX ...
...nd similar story for trying to change the write protection values from true to false for all flash sectors: 16:26:41:386 : Error: Expected value for Option Byte "WRP0": 0x0, found: 0x1
16:26:41:3...