Hi Team, In this module(TESEO-LIV4f) can able to processing the data L5 band(NACIC data and IRNSS) And how to update the firmware for l5 band(navic and Irns...
Hello I need to use full featured Teseo-Suite. Sending letters to st-teseo-suite-support@st.com remain unanswered. How could I obtain a full version of Teseo-Suite? Thanks
Hello, I'm using a Teseo III module from Lantronix. When connected up, I can see NMEA sentences over UART, at 9600 baud. I have a few questions. I'm not a GPS expert, and unfortunately, the Teseo I...
Hello, In document UM3009 §7.3 => Multi-constellation firmware supports the following constellations: GPS, GALILEO, GLONASS, BEIDOU and QZSS. All constellations cannot be enabled at the s...
Hello I am interested at looking at the Teseoo-LIV3F for a application but I require a very fast TTFF. Having read up on the A-GNSS option will this be available any where or any location in t...
Hi, We're attempting to update the LIV4F firmware via the UART interface from an embedded device, however, we're unable to replicate the steps documented in UM3009. Our code works up until ...
Hello,
I am currently working with the NUCLEO GNSS2A1 extension on the NUCLEO-L010RB demonstration board, and I am trying to retrieve data from the gyroscope and accelerometer.
Acc...
While researching the GNSS module for my project, I got somewhat confused about the power connection of the LIV4F module due to inconsistent information in the manuals. The general recommendation is ...
I made a PCB using Teseo-LIV3F as stand alone, tried to connect TX and RX of the module to Arduino TX and RX using I TinyGps++ library, but I couldn't get any response from the module. I tried to con...