STM32 MPUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157F GRUB boot command line

I would like to only use cgroup v2 and would like to modify the kernel cmdline boot arguments as follows:, .  I searched internet and suggestion is to useadd systemd. unified_cgroup_hierarchy=1 under /etc/default/grub , followed by sudo update-grub ....

pme991 by Associate II
  • 117 Views
  • 1 replies
  • 0 kudos

X-STM32MP-GNSS2 board - Linux

Hello, I have the STM32MP157-DK2 board and the GNSS2 eval board (w/Taoglas antenna) and I am trying to follow UM2909 (getting started).  It seems the ST Wiki is updated past the UM2909.  For example  in 3.3 titled “Downloading the kernel sources (dev...

rick2399 by Associate II
  • 164 Views
  • 1 replies
  • 0 kudos

Resolved! Qt SDK build failed with turorial

Hey, I'm following the Distribution Package tutorial, specifically the QT image and SDK with EGLFS tutorial: wiki  I did build the Qt image with     bitbake st-example-image-qt     but building the SDK with     bitbake st-example-image-qt -c populate...

oli1 by Associate II
  • 1077 Views
  • 4 replies
  • 2 kudos

How to start M4 on startup of STM32MP1?

I realize this is probably a pretty basic question but I haven't found a way to have the M4 portion of the firmware startup when the STM32MP1 is powered up.  I'm currently using an STM32MP157D-DK1 board, if that helps. I was able to debug the code of...

JayDev by Senior II
  • 1905 Views
  • 3 replies
  • 0 kudos

Resolved! How do I open a uboot shell?

I know this is probably a really stupid/noob question but I was trying to flash the STM32MP157D-DK1 board I have for the first time following the following guide:https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package I ran into ...

JayDev by Senior II
  • 3237 Views
  • 10 replies
  • 0 kudos