GPIO port documentation query: P-MOS is shown inverted but is active high, and vice versa for N-MOS
- October 24, 2023
- 2 replies
- 3050 views
With reference to RM0436, the STM32MP157 Reference Manual, revision 6.
On pages 1066 and 1072 the schematic structures of a GPIO port are drawn (figures 119, 120, and 122). These all show an inverter circle on the gate of P-MOS output transistor and none on the N-MOS transistor. This suggests that the P-MOS is active low and the N-MOS is active high.
However, the written documentation states the opposite: that the P-MOS is active high (pulls the output pin high for a "1" bit unless in open-drain mode) and the the N-MOS is active low (pulls the output pin low for a "0" bit).
From experience I believe that the written documentation is correct, so should the schematic not be redrawn to show the inverter circle on the gate of the N-MOS output transistor?
Attached please find annoted screen shots of the pages in question.