2023-10-04 4:38 PM
I know this is probably a really stupid/noob question but I was trying to flash the STM32MP157D-DK1 board I have for the first time following the following guide:
https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package
I ran into an issue where it started the flash and then couldn't reconnect. I did find this article that seems to describe exactly the issue I'm having:
It recommends:
In Uboot shell run a Dfu command :
STM32MP> env set dfu_alt_info "DDR ram 0xC0000000 0x20000000"
STM32MP> dfu 0 ram 0
Unfortunately, I don't know how to run a uboot shell to try this. I know this is probably a really stupid problem . . . but I'm also hoping that means it has an easy solution as well. Any help you can give me would be greatly appreciated. Thanks!
Solved! Go to Solution.
2023-10-17 1:08 AM
Hi @JayDev ,
Did you tried another USB port on your PC, thru an USB hub ? With another PC, another USB cable ?
Maybe details your PC setup (W10 ? W11 ? USB-A or USB-C port ? ...)
Regards.
2023-10-04 5:54 PM
I do have a ST-Link to the board and I'm watching the serial port @ 115200 and can see info coming in, I just don't know how to actually get to the u-boot to change the command. Maybe I'm getting closer but I'm not 100% sure. Thanks!
2023-10-05 1:00 AM
Hi @JayDev
to reach uboot prompt, simply press a key on the serial console at right time during boot sequence.
.....
U-Boot 2022.10-stm32mp-r1 (Oct 03 2022 - 19:25:32 +0000)
CPU: STM32MP157FAC Rev.Z
Model: STMicroelectronics STM32MP157F-DK2 Discovery Board
Board: stm32mp1 in trusted mode (st,stm32mp157f-dk2)
Board: MB1272 Var4.0 Rev.C-02
DRAM: 512 MiB
optee optee: OP-TEE: revision 3.19 (afacf356)
Clocks:
- MPU : 800 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
Core: 367 devices, 43 uclasses, devicetree: board
WDT: Started watchdog with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
Net: eth0: ethernet@5800a000
Hit any key to stop autoboot: 0
STM32MP>
Regards.
2023-10-09 12:39 PM
So, I've been trying to get this to work but still haven't seen the boot. I've tried plugging in the USB power and USB Micro/STLink and clicking the reset button but get no output. I've tried leaving STLink plugged in and resetting (both end up with LD6 blinking red on and off. I can plug in the other USB-C connector and the light goes solid. Still no output, even when resetting.
The only time I can get an actual output is when trying to program the device over USB in STM32Prog. This is the output screen I'm getting:
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0xde000000
INFO: Image id=4 loaded: 0xde000000 - 0xde00001c
INFO: OPTEE ep=0xde000000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x1
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0xde000000
INFO: Image id=8 loaded: 0xde000000 - 0xde036b68
INFO: BL2: Skip loading image id 9
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0500000
INFO: Image id=2 loaded: 0xc0500000 - 0xc051ee40
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01f5d3c
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0xde000000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC:
I/TC: Embedded DTB found
I/TC: OP-TEE version: 3.19.0-dev (gcc version 12.2.0 (GCC)) #1 Fri Oct 14 19:00:05 UTC 2022 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp157d-dk1.dts
I/TC: DTB enables console (non-secure)
I/TC: Primary CPU switching to normal world boot
optee optee: OP-TEE: revision 3.19 (afacf356)
U-Boot 2022.10-stm32mp-r1 (Oct 03 2022 - 19:25:32 +0000)
CPU: STM32MP157DAC Rev.Z
Model: STMicroelectronics STM32MP157D-DK1 Discovery Board
Board: stm32mp1 in trusted mode (st,stm32mp157d-dk1)
Board: MB1272 Var3.0 Rev.C-02
DRAM: 512 MiB
optee optee: OP-TEE: revision 3.19 (afacf356)
Clocks:
- MPU : 800 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
Core: 359 devices, 39 uclasses, devicetree: board
WDT: Started watchdog with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0
Loading Environment from nowhere... OK
In: serial
Out: serial
Err: serial
Previous ADC measurements was not the one expected, retry in 20ms
****************************************************
* ERROR USB TYPE-C connection in unattached mode *
* Check that USB TYPE-C cable is correctly plugged *
* Current too low, use a 3A power supply! *
****************************************************
All signs appear to be pointing to the power supply, but that doesn't make sense to me as I'm currently using a 5V 3A supply (I'm using https://www.mouser.com/ProductDetail/TT-Electronics-IoT-Solutions/T7715DV?qs=vLWxofP3U2zWk%2FI5z4EHKA%3D%3D ). Is it possible the issue really is the power supply? Maybe it's dipping and browning out? Or is my current process for getting to uboot incorrect?
Thanks for your help and sorry for the delay! I should be faster to respond this week!
2023-10-09 1:42 PM
Ok, since the last post, I went and found a phone charger (which likely has better USB protocols than a straight USB C 3A charger. It seemed to get past the previous issue so I was able to get into the boot mode and quickly type in
STM32MP> env set dfu_alt_info "DDR ram 0xC0000000 0x20000000"
STM32MP> dfu 0 ram 0
Now the issue I'm having is it seems to be timing out before it finishes programming the board. This is what I'm seeing:
STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp157d-dk1-optee.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 001F00283438511536383238
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP15xx
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157d-dk1-usb.stm32
File : tf-a-stm32mp157d-dk1-usb.stm32
Size : 220.40 KB
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:02.588
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Memory Programming ...
Opening and parsing file: fip-stm32mp157d-dk1-optee.bin
File : fip-stm32mp157d-dk1-optee.bin
Size : 1.29 MB
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:01.771
RUNNING Program ...
PartID: :0x03
Reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157DAC Rev.Z,
SN : 001F00283438511536383238
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP157DAC Rev.Z
Device type : MPU
Device CPU : Cortex-A7
Start operation done successfully at partition 0x03
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157DAC Rev.Z,
SN : 001F00283438511536383238
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP157DAC Rev.Z
Device type : MPU
Device CPU : Cortex-A7
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157d-dk1-sdcard.stm32
File : tf-a-stm32mp157d-dk1-sdcard.stm32
Size : 220.42 KB
Partition ID : 0x04
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.171
RUNNING Program ...
PartID: :0x04
Start operation done successfully at partition 0x04
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157d-dk1-sdcard.stm32
File : tf-a-stm32mp157d-dk1-sdcard.stm32
Size : 220.42 KB
Partition ID : 0x05
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.184
RUNNING Program ...
PartID: :0x05
Start operation done successfully at partition 0x05
Memory Programming ...
Opening and parsing file: metadata.bin
File : metadata.bin
Size : 96.00 B
Partition ID : 0x06
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.006
RUNNING Program ...
PartID: :0x06
Start operation done successfully at partition 0x06
Memory Programming ...
Opening and parsing file: metadata.bin
File : metadata.bin
Size : 96.00 B
Partition ID : 0x07
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.006
RUNNING Program ...
PartID: :0x07
Start operation done successfully at partition 0x07
Memory Programming ...
Opening and parsing file: fip-stm32mp157d-dk1-optee.bin
File : fip-stm32mp157d-dk1-optee.bin
Size : 1.29 MB
Partition ID : 0x08
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:01.085
RUNNING Program ...
PartID: :0x08
Start operation done successfully at partition 0x08
Memory Programming ...
Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
File : st-image-bootfs-openstlinux-weston-stm32mp1.ext4
Size : 64.00 MB
Partition ID : 0x10
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:59.657
RUNNING Program ...
PartID: :0x10
Start operation done successfully at partition 0x10
Memory Programming ...
Opening and parsing file: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
File : st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
Size : 16.00 MB
Partition ID : 0x11
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:14.982
RUNNING Program ...
PartID: :0x11
Start operation done successfully at partition 0x11
Memory Programming ...
Opening and parsing file: st-image-weston-openstlinux-weston-stm32mp1.ext4
File : st-image-weston-openstlinux-weston-stm32mp1.ext4
Size : 586.38 MB
Partition ID : 0x12
Download in Progress:
[====== ] 12%
Error: failed to download data chunck [0]
Error: failed to download Segment[0]
Error: failed to download the File
Error: Download partition 0x12 failed
Error: TSV flashing service failed
Any ideas how to get around this issue? I'm not entirely sure how to change the timeout. I've essentially got the same result from the STM32 Programmer and from the CLI tool.
Thanks!
2023-10-10 12:36 AM
Hi @JayDev ,
Could you please try to replace in tsv :
- 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157d-dk1-usb.stm32
- 0x03 fip-boot FIP none 0x0 fip/fip-stm32mp157d-dk1-optee.bin
by
- 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157a-dk1-usb.stm32
- 0x03 fip-boot FIP none 0x0 fip/fip-stm32mp157a-dk1-optee.bin
Let me know the result
Thanks
Olivier
2023-10-11 9:10 AM
Well, the good news is I got a different outcome but I'm not entirely sure what that tells me, to be honest (though you likely do).
To be clear, my edited file currently looks like this (for confirmation):
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157a-dk1-usb.stm32
- 0x03 fip-boot FIP none 0x0 fip/fip-stm32mp157a-dk1-optee.bin
P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157d-dk1-sdcard.stm32
P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157d-dk1-sdcard.stm32
P 0x06 metadata1 FWU_MDATA mmc0 0x00084400 arm-trusted-firmware/metadata.bin
P 0x07 metadata2 FWU_MDATA mmc0 0x000C4400 arm-trusted-firmware/metadata.bin
P 0x08 fip-a FIP mmc0 0x00104400 fip/fip-stm32mp157d-dk1-optee.bin
PED 0x09 fip-b FIP mmc0 0x00504400 none
PED 0x0A u-boot-env ENV mmc0 0x00904400 none
P 0x10 bootfs System mmc0 0x00984400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P 0x11 vendorfs FileSystem mmc0 0x04984400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P 0x12 rootfs FileSystem mmc0 0x05984400 st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x13 userfs FileSystem mmc0 0x105984400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
Below is what my output was. Note it made it to 48% rather than the previous 12% and seems to have failed with chunk 2 instead of chunk 0.
STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/optee/EDIT_FlashLayout_sdcard_stm32mp157d-dk1-optee.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 001F00283438511536383238
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP15xx
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157a-dk1-usb.stm32
File : tf-a-stm32mp157a-dk1-usb.stm32
Size : 220.40 KB
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:02.557
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Memory Programming ...
Opening and parsing file: fip-stm32mp157a-dk1-optee.bin
File : fip-stm32mp157a-dk1-optee.bin
Size : 1.29 MB
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:01.745
RUNNING Program ...
PartID: :0x03
Reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157DAC Rev.Z,
SN : 001F00283438511536383238
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP157DAC Rev.Z
Device type : MPU
Device CPU : Cortex-A7
Start operation done successfully at partition 0x03
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157DAC Rev.Z,
SN : 001F00283438511536383238
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP157DAC Rev.Z
Device type : MPU
Device CPU : Cortex-A7
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157d-dk1-sdcard.stm32
File : tf-a-stm32mp157d-dk1-sdcard.stm32
Size : 220.42 KB
Partition ID : 0x04
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.195
RUNNING Program ...
PartID: :0x04
Start operation done successfully at partition 0x04
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157d-dk1-sdcard.stm32
File : tf-a-stm32mp157d-dk1-sdcard.stm32
Size : 220.42 KB
Partition ID : 0x05
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.203
RUNNING Program ...
PartID: :0x05
Start operation done successfully at partition 0x05
Memory Programming ...
Opening and parsing file: metadata.bin
File : metadata.bin
Size : 96.00 B
Partition ID : 0x06
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.006
RUNNING Program ...
PartID: :0x06
Start operation done successfully at partition 0x06
Memory Programming ...
Opening and parsing file: metadata.bin
File : metadata.bin
Size : 96.00 B
Partition ID : 0x07
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.006
RUNNING Program ...
PartID: :0x07
Start operation done successfully at partition 0x07
Memory Programming ...
Opening and parsing file: fip-stm32mp157d-dk1-optee.bin
File : fip-stm32mp157d-dk1-optee.bin
Size : 1.29 MB
Partition ID : 0x08
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:01.182
RUNNING Program ...
PartID: :0x08
Start operation done successfully at partition 0x08
Memory Programming ...
Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
File : st-image-bootfs-openstlinux-weston-stm32mp1.ext4
Size : 64.00 MB
Partition ID : 0x10
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:01:04.933
RUNNING Program ...
PartID: :0x10
Start operation done successfully at partition 0x10
Memory Programming ...
Opening and parsing file: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
File : st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
Size : 16.00 MB
Partition ID : 0x11
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:16.113
RUNNING Program ...
PartID: :0x11
Start operation done successfully at partition 0x11
Memory Programming ...
Opening and parsing file: st-image-weston-openstlinux-weston-stm32mp1.ext4
File : st-image-weston-openstlinux-weston-stm32mp1.ext4
Size : 586.38 MB
Partition ID : 0x12
Download in Progress:
[======================== ] 48%
Error: failed to download data chunck [2]
Error: failed to download Segment[0]
Error: failed to download the File
Error: Download partition 0x12 failed
Error: TSV flashing service failed
2023-10-11 9:21 AM
If it helps, I also just tried to run:
STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp157a-dk1-optee.tsv
It appears this time it failed at 50% of chunk 0x12 and gave the following output:
Memory Programming ...
Opening and parsing file: st-image-weston-openstlinux-weston-stm32mp1.ext4
File : st-image-weston-openstlinux-weston-stm32mp1.ext4
Size : 586.38 MB
Partition ID : 0x12
Download in Progress:
[========================= ] 50%
Error: failed to download data chunck [3]
Error: failed to download Segment[0]
Error: failed to download the File
Error: Download partition 0x12 failed
Error: TSV flashing service failed
2023-10-16 4:55 PM
Any other ideas on where to proceed from here? I'm running out of ideas, unfortunately. Anything else I can try to get more information?
2023-10-17 1:08 AM
Hi @JayDev ,
Did you tried another USB port on your PC, thru an USB hub ? With another PC, another USB cable ?
Maybe details your PC setup (W10 ? W11 ? USB-A or USB-C port ? ...)
Regards.