Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Machine learning using stm32h755 chip

I am trying to integrate the a neural network machine learning model into the stm32h755 chip. I downloaded the stmCubeMx, installed X-Cube-Ai, selected the core, added the network using tflite file and then generated the code. I can't find the ai_mod...

slodh by Associate II
  • 1980 Views
  • 9 replies
  • 0 kudos

Validation on Target can't get my device

I'm a senior student majored in AI before and recently bought an STM32H743VIT6 to experiment with Edge AI. I haven't had any experience with embedded systems before. My ports seem to be missing, but CubeProgrammer successfully found my device through...

QQ图片20241024105216.png
Zilliax by Associate
  • 564 Views
  • 2 replies
  • 0 kudos

Deploying tensorflowlite object detection model

Hi, I am using STM32F746G Discovery Board to deploy an object detection model to detect person in an image. The model size of the object detection model is less than 1Mb. The implementation would be like to make an inference in the microcontroller li...

modulo3see_0-1729244958648.png

ROM overflowed with over 3000 kB tflite models on ISPU

I am testing a tflite model on the ISPU, using the following hardware:NUCLEO-F401RE + X-NUCLEO-IKS4A1I downloaded the x-cube-ispu repo and imported the template_stedgeai example to STM32CubeIDE. Finally i generate the network library with:  stedgeai ...

konaukko by Associate
  • 738 Views
  • 1 replies
  • 0 kudos

STM32H747I DISCO : model zoo object-detection memory areas

Hello there,I'm using stm32h747i-DISCO board, and running object detection demo from model-zoo. Now i want to add Ethernet functionality with the demo. I have some questions for the same, as below...Q1) there is only one linker script in object detec...

image (4).png

Resolved! ML algorithms used in nanoedge MC classification

Hi,1) I Am currently exploring the capabilities of NanoEdge for a project involving multiclass classification, and I am eager to learn more about the specific machine learning algorithms utilized within the NanoEdge framework. I feel as though I am u...

martur by Associate
  • 647 Views
  • 1 replies
  • 0 kudos

Resolved! "Correct" Way to Gather Data and Train ML for IMU

I am lost in the maze of documentation for AI features at STM. I have access right now to:STEVAL-MKBOXPRO (SensorTile.box PRO)Custom board with LSM6DSV16XI want to:gather IMU data to train the modeltrain the IMU device decision tree classifier (3 cla...

Resolved! Lis2duxs12 Qvar - touch ucf and power consumption questions

 1. Is there a ucf file or setup description for touch or swipe ? 2. The power consumption seems very high for touch and swipe. Using the adapter board and Unico, with just the accelerometer and qvar running at 200hz low power mode, its about 13uA. I...

Resolved! NanoEdge AI Studio updates

Dear STM,is there a way to avoid the installation of a new version of NanoEdge AI when a new version is available ?Or maybe to pospone the installation ?When a new version is available I got a dialog Win like the one below, if I click on Exit then th...

MaxC_0-1728993958617.png
MaxC by Associate III
  • 703 Views
  • 2 replies
  • 1 kudos